Feedback_Boost_Current

Index.Sub 2230.12H
Data Type Unsigned16
Access Read/Write
PDO Mappable

RX_PDO (1)

Unit

milliamperes (mA)

Range

0 ÷ (max drive current)
Default Value 1500
Store Supported Yes
Description This value is used for Closed Loop feature and defines maximum current supplied to the motor. The parameter is also used to limit the motor torque.

Notes

(1) available with firmware V00r75 or superior.